OperationErrsCt

The
OperationErrsCt
item returns the number of equipment operation sequence errors currently detected by the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input Format
Request:
OperationErrsCt
Output Format
The OperationErrsCt item returns in this format:
<NumberOfErrors>
Field Name
Format
Description
<NumberOf
Errors>
ASCII - Integer
Number of equipment operation sequence errors currently detected by the
FactoryTalk Batch
Server.
This table shows an example of the return on this request.
Example:
A request on
object.GetItem(OperationErrsCt)
could return:
3
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal