PhaseIDPausing
The
PhaseIDPausing
item returns the PAUSING attribute for a phase or an equipment operation sequence.This table shows the input and output formats for this item.
Input Format | Request: PhaseIDPausing | ||
PhaseID | is | Unique equipment ID corresponding to the phase or equipment operation sequence. | |
Output Format | The PhaseIDPausing item returns in this format: <PausingText> | ||
Field Name | Format | Description | |
<PausingText> | ASCII - String | Value in the Pausing tag in the process-connecteddevice (PCD).
| |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(68Pausing) could return:Off |
Provide Feedback