Locale

The
Locale
item returns the locale information used by the
FactoryTalk Batch
Server. This includes the language ID and code page.
This table shows the input and output formats for this item.
Input Format
Request:
Locale
Output Format
The Locale item returns in this format:
<LanguageID>
\t
<CodePage>
Field Name
Format
Description
<LanguageID>
ASCII – String
ID that identifies the language:
1031 – German (Standard)
1033 – English (United States)
1036 – French (Standard)
1040 – Italian (Standard)
3082 – Spanish (Modern Sort)
<CodePage>
ASCII – String
Code page used by server, decimal number
This table shows an example of the return on this request.
Example:
A request on
object.GetItem(Locale)
could return:
1033 \t 1252
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal