InfoMessage

The
InfoMessage
item returns the most recent information message in the
FactoryTalk Batch
Server’s log file.
This table shows the input and output formats for this item.
Input Format
Request:
InfoMessage
Output Format
The InfoMessage returns in the format:
<Time>
\t
<Description>
\t
<Additional Data>
where:
Field Name
Format
Description
<Time>
ASCII – String
Time when the message generated.
<Description>
ASCII – String
General description of the message.
<Additional Data>
ASCII – String
More specific message information. May be <NullString> or a blank space character <sp>.
This table shows an example of the return on this request.
Example:
A request on
object
.
GetItem(InfoMessage)
could return:
2022.02.24 16:20:56:488 \t COMMAND VALUE UPDATE RECEIVED - COMMAND NOT YET PROCESSED BY PHASE \t CMDID =1 LOW BYTE =100 \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal