ResourceIDOwned
The
ResourceIDOwned
item returns a resource list and their associated equipment IDs, which are currently owned by the resource denoted as ResourceID
. A resource must be configured as a needed equipment item in FactoryTalk Batch Equipment Editor
or must be specifically requested by the phase logic in order to be considered owned. The resource ID for the operator is 0
.This table shows the input and output formats for this item.
Input Format | Request: ResourceIDOwned | ||
ResourceID | is | ASCII - String, the | |
Output Format | The ResourceIDOwned item returns in this format: | ||
<ResourceIDOwned> | is | <NullList> \crlf | <OwnedList> \crlf | |
<OwnedList> | is | <Resource> | <Resource> <OwnedList> | |
<Resource> | is | <ResourceID> \t <ResourceName> \crlf | |
where: | |||
Field Name | Format | Description | |
<ResourceID> | ASCII - Integer | Unique equipment ID configured in FactoryTalk Batch Equipment Editor . | |
<ResourceName> | ASCII - String | Name of the Procedure, Process Cell, Unit, Phase or Resource. | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(68Owned) could return:125 \t P101 \crlf |
Provide Feedback