RunWithoutMatSvr

The
RunWithoutMatSvr
item returns the configured option of running when Material Server communication is lost as an ordinal data item.
This table shows the input and output formats for this item.
Input Format
Request:
RunWithoutMatSvr
Output Format
The RunWithoutMatSvr item returns in this format:
<Option>
where:
Field Name
Format
Description
<Option>
ASCII - Integer
0 = FailureAndHold
1 = SwitchToManual
This table shows an example of the return on this request.
Example:
A request on
object
.
GetItem(RunWithoutMatSvr)
could return:
1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal