COMClientCount

The
COMClientCount
item returns the number of COM clients connected to the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input Format
Request:
COMClientCount
Output Format
The COMClientCount item returns in this format:
<COMCount>
Field Name
Format
Description
<COMCount>
ASCII – String
Number of COM clients connected to the
FactoryTalk Batch
Server.
This table shows an example of the return on this request.
TIP:
A request on
object
.
GetItem(COMClientCount)
could return:
3
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal