EquipmentModelUpdateVersion

The
EquipmentModelUpdateVersion
item returns an integer value. This integer value is incremented by one every time a runtime area model update is successfully performed.
This table shows the input and output formats for this item.
Input Format
Request:
EquipmentModelUpdateVersion
Output Format
The
EquipmentModelUpdateVersion
item returns data in this format:
<Version>
Field Name
Format
Description
<Version>
ASCII – Integer
Current runtime area model update version.
This table shows an example of the return on this request.
TIP:
A request on object.GetItem(EquipmentModelUpdateVersion) could return:
17
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal