EnumSetEnumSet
The
EnumSetEnumSet
item returns the names and ordinal values for each enumeration within the specified enumeration set as defined in the current area model.This table shows the input and output formats for this item.
Input Format | Request only: EnumSetEnumSet | ||
EnumSet | is | ASCII – text, any enumeration set name as defined in the equipment database. | |
Output Format | The EnumSetEnumSet item returns in this format: | ||
<EnumList> | is | <EList> | <EList> <EnumList> | |
<EList> | is | <EnumName> \t <OrdValue> \crlf | |
Field Name | Format | Description | |
<EnumName> | ASCII – String | Enumeration name. | |
<OrdValue> | ASCII – String | Ordinal value associated with the enumeration. | |
This table shows an example of the return on this request.
TIP:
A request on
object.GetItem(YES_NOEnumSet)
could return:NO \t 0 \crlf
YES \t 1 \crlf
Provide Feedback