UnitIDPhases
The
UnitIDPhases
item returns a list of all the phases within the unit specified by the unit ID.This table shows the input and output formats for this item.
Input Format | Request: UnitIDPhases | ||
UnitID | is | An ASCII - Integer representing the | |
Output Format | The UnitIDPhases item returns in this format: | ||
<PhaseList> | is | <Phase> \crlf <Phase> \crlf <PhaseList> | |
<Phase> | is | <PhaseID> \t <PhaseName> \t <MaxOwners> \t <XCord> \t <Ycord> \t <BitMapIndex> | |
where < Phase > is: | |||
Field Name | Format | Description | |
<PhaseID> | ASCII - Integer | Phase’s resource ID. | |
<PhaseName> | ASCII - String | Phase name. | |
<MaxOwners> | ASCII - Integer | Maximum number of owners. | |
<XCord> | ASCII - Integer | X coordinate for the bitmap in the Equipment View | |
<YCord> | ASCII - Integer | Y coordinate for the bitmap in the Equipment View. | |
<BitMapIndex> | ASCII - Integer | Location of bitmap in the List of Phase Bitmap items. | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(55Phases) returns:68 \t NP_ADDDAIRY_M1 \t 1 \t 95 \t 88 \t 1 \crlf 70 \t NP_ADDEGG_M1 \t 1 \t 362 \t 89 \t 2 \crlf 72 \t NP_HEAT_M1 \t 1 \t 343 \t 182 \t 3 \crlf 71 \t NP_AGITATE_M1 \t 1 \t 235 \t 183 \t 4 \crlf 73 \t NP_XFR_OUT_M1 \t 1 \t 233 \t 362 \t 5 \crlf |
Provide Feedback