ResourceIDHyperlinks

The
ResourceIDHyperlinks
item returns a tab-delimited list of hyperlinks that were configured in the area model for the equipment element identified by the resource ID.
This table shows the input and output formats for this item.
Input Format
The
FactoryTalk Batch
Server supports an item named
ResourceIDHyperlinks
.
The format of the data returned by this item is:
<ResourceName>
\t
<Hyperlink1>
\t
<Hyperlink2>
\t
<Hyperlink3>
\t
<Hyperlink4>
\t
<Hyperlink5>
Output Format
The ResourceIDHyperlinks item returns in this format:
where:
Field Name
Format
Description
ResourceName
ASCII - String
Resource name identified by the ResourceID included in the item. Can represent a process cell, unit, equipment phase or shared resource.
Hyperlink#
ASCII - String
Hyperlinks defined for the identified resource, where
#
is a number from 1 through 5. An empty string returns for any hyperlink without an assigned a value in the area model.
This table shows an example of the return on this request.
Example:
A request on
object
.
GetItem(68Hyperlinks)
could return:
NP_ADDDAIRY_M1 \t HYPERLINK1 \t HYPERLINK2 \t HYPERLINK3 \t HYPERLINK4 \t HYPERLINK5
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal