Single Specific Ingredient Addition Phase with Multiple Lot IDs

This is an example of Single Specific Ingredient Addition Phase with Multiple Lot IDs:
Formula Parameter:
Material_Oil
Formula Parameter:
Setpoint_Oil
Report Parameter:
Lot_Oil_01
Report Parameter:
Lot_Oil_02
Report Parameter:
Actual_Lot_Oil_01
Report Parameter:
Actual_Lot_Oil_02
Report Parameter:
Target_Oil
Report Parameter:
Actual_Oil
Report Parameter:
In_Tolerance_Oil
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal