Improved implementation of phase logic routines

Logix Designer
with
PhaseManager
improves the implementation of equipment phases in
Logix 5000
controllers. Using OPC and the PLI, a phase is typically executed in a single relay ladder logic (RLL) routine that implements logic for all of the active states defined by the S88 standard. These active states include Stopping, Starting, Running, Holding, Aborting, and Restarting.
TIP:
PhaseManager
also provides an additional active state in
Logix Designer
, Resetting, which can be used for other types of projects not based on the S88 standard.
PhaseManager
supports a modularized approach to developing state routine logic by facilitating the development of each active state in its own routine.
PhaseManager
represents an equipment phase as a type of program in
Logix Designer
. Since programs can contain multiple routines, develop a separate routine for each active state required for the equipment phase. Developing separate routines for each active state also provides the ability to develop each routine in different programming languages.
Use other
Logix Designer
program features when developing equipment phase logic. These features include the ability to use timing diagnostics information, Max and Last Scan, for debugging equipment phases in
Logix Designer
, and the ability to configure a fault routine for the equipment phase.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal