Add enumeration members
    Use these instructions to add enumeration members.
To add enumeration members
:- SelectStart > Rockwell Software > Equipment Editor.
- SelectEdit > Enumeration Setsto open theCreate Enumeration Sets and Enumerationsdialog box.
- Select the enumeration set.
- UnderEnumerations, selectNew.TIP:Members to the system enumeration sets cannot be added: YES_NO, MATERIALS, MATERIAL_CLASSES, and CONTAINERS.
- Type the enumeration name and the ordinal value, or accept the default ordinal value.IMPORTANT:PHASE_FAILURES enumerations only support positive ordinals from 0 through 32767.
- SelectOKto return to theCreate Enumeration Sets and Enumerationsdialog box. The new enumeration name displays underEnumerations.
Provide Feedback