Unable to access instruction file

The XML schema requires that the contents of any instruction files must be included in the XML file.
FactoryTalk Batch Equipment Editor
must access the instruction file at the time of the export. If the instruction files cannot be accessed, this error message displays and the export does not occur.
FTB_EE_XML_export_InstrFileNotFound
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal