Download all parameters (input parameters)
Configure the PXRQ instruction in
Logix Designer
to download values for all configured input parameters to the input parameter array:External Request | Data Value Array Element | Value |
|---|---|---|
Download Input Parameters | DINT[0] | 0 |
If control strategies are enabled, only those parameters assigned to the recipe’s control strategy will be downloaded. The control strategy parameter is Parameter1.
Provide Feedback