Download parameters (input parameters) request

During batch execution, phase logic can send a request to the
FactoryTalk Batch
Server to download all input parameter values, a single input parameter value, or a range of input parameter values, including phase parameter limits that exist.
The parameter values may be specified when adding a phase to a recipe using
FactoryTalk Batch Recipe Editor
. If the phase parameter value is not specified when the recipe is built, the
FactoryTalk Batch
Server sends
FactoryTalk Batch View
a request for the value when a
Download Input Parameters
or
Download Input Parameters Subset
request is received from the phase.
FactoryTalk Batch View
requests the phase parameter value from the operator by way of an Unacknowledged Prompt.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal