Configure a custom archiver
Configure the custom archiver from the Equipment Editor.
To configure a custom archiver
:- In the Equipment Editor, selectOptions > Server Options.
- In theServer Optionsdialog box, select theBatch Reportingtab.
- SelectUser-defined (End of Batch).
- InExecutable File, select browse (
) and locate the custom archiver's .exefile. - InInitialization File, select browse (
) and locate the custom archiver's initialization .inifile. - SelectOK.
Provide Feedback