FactoryTalk Batch View HMI Controls

The
FactoryTalk® Batch View
HMI controls provide an interface that allows users to monitor and interact with the production process within a
FactoryTalk View SE
Display Client. The
FactoryTalk Batch
View HMI controls consist of:
  • BatchesList control: Creates control recipes, displays current control recipes, and commands a control recipe. In FactoryTalk View SE, shown as
    BatchesList
    control
    BatchViewHMI.BatchesList
    in the
    Insert an ActiveX Control
    dialog box and the
    Property Panel
    .
  • PromptsList control: Displays a list of prompts that are waiting to be acknowledged, a list of electronic signatures associated with a batch that are waiting for signoff, and instructions waiting to be acknowledged. In FactoryTalk View SE, shown as
    PromptsList
    control
    BatchViewHMI.PromptsList
    in the
    Insert an ActiveX Control
    dialog box and the
    Property Panel
    .
  • SFC control: Enables the ability to command batches during
    FactoryTalk View SE
    runtime on the Details and Summary pages of the SFC. In FactoryTalk View SE, shown as
    SFC
    control
    BatchViewHMI.SFC
    in the
    Insert an ActiveX Control
    dialog box and the
    Property Panel
    .
  • Full control: Accesses the entire
    FactoryTalk Batch View
    site. In
    FactoryTalk View SE
    , shown as
    Full
    control
    BatchViewHMI.FullView
    in the
    Insert an ActiveX Control
    dialog box and the
    Property Panel
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal