Set report preferences
You can define a footer to print on each report page and select the font and color (if your printer supports color printing) for the various report sections.
To set report preferences
:- From theViewmenu, selectUser Preferences. TheUser Preferencesdialog box opens to theGeneraltab.
- Select theReportstab. The default report style for most views isFormatted.
- To change the type of printed report, select eitherListorFormattedto the right of the appropriate report.TIP:If you select theListformat, set the page orientation to landscape. From theFilemenu, selectPrint Setup, selectLandscapein the Orientation area, and then clickOK.
- Where available, you can selectInclude Related Data,and any additional data associated with the selected item (single items only – not lists or groups) also prints on the report.
- In theFooter Textbox, type a word or phrase to appear centered at the bottom of each page.
- ClickApply.
Provide Feedback