Synchronize to create phases in the area model
Use these instructions to synchronize the area model to create phases.
Prerequisites:
- InstallLogix DesignerandFactoryTalk Linxon the same computer asFactoryTalk Batch Equipment Editor.
- If the new phase is not added to an existing unit, create a unit to contain the new phase inFactoryTalk Batch Equipment Editor. Create a project file inLogix Designerand define equipment phases.
- In the area model, define aLogix5000CIP data server for theLogix5000controller that is connected to the new machine, and specify this project file. (SeeAdd afor more information.)Logix5000CIP data server
- In the area model, configure a unit instance to add the new phase to and aLogix5000CIP data server for the controller specified in the project file.
To synchronize to create phases in the area model:
- Save the area model and select a data server to synchronize.
- Select the phases to create in the area model.
- Select a phase class and unit for the new phase and synchronize.ORCreate a new phase class for the phase, select a unit, and synchronize.
All synchronization steps are completed in
FactoryTalk Batch Equipment Editor
.Provide Feedback