FactoryTalk Event Archiver Service

FactoryTalk Event Archiver
runs as a Windows service. Assign a Windows user account to the Archiver Service to log on to the system. By default, the Archiver Service uses the
FactoryTalk Batch
Server user account specified during the installation. If archiving data to the local computer only, use the Local System account instead of the server user account.
IMPORTANT:
On Windows Server systems using Active Directory, change the default format of
user@domain.com
to
domain\user
.
The
FactoryTalk Event Archiver
cannot access the database if the database account name has special characters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal