Download one attribute of a material

Configure the PXRQ instruction in
Logix Designer
to download one attribute of a material to a specified tag. The attribute identified by the attribute ID downloads into the parameter ID specified.
Download
Material Manager
Database Data
DINT[0]
0
DINT[1]
Parameter ID material data will be downloaded to.
DINT[2]
Material Controller ID
DINT[3]
Attribute ID
TIP:
The data type in the controller must match the data type of the parameter ID specified in the data value array element DINT[1].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal