Unable to access Material Server for material support

There is a requirement that material support per container must be included in the XML file.
FactoryTalk Batch Equipment Editor
must make a call to the Material Server at the time of the export. It is possible that the Material Server cannot be accessed at that time.
If the Material Server cannot be accessed, this error message displays and the export does not occur.
FTB_EE_XML_export_NoMatlServer
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal