Network Editor

The Network Editor is a utility that allows you to indicate where other ®
FactoryTalk® Batch
Batch and/or
FactoryTalk Batch
Material Manager
Servers are located on the network. This network configuration information simplifies integration with other
FactoryTalk
products and the process of reconfiguring a multi-computer system.
During installation, the network configuration information is completed based on your responses. If you have multiple servers in your network, use the Network Editor to update the location of all your servers.
The Network Editor is installed automatically with the
FactoryTalk Batch
and Material Servers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal