Verify and deploy an updated area model using the FactoryTalk Batch Service Manager

To prepare an online area model for deployment, an operator can verify that changes made to the area model are permitted.
TIP:
You will be asked to login to FactoryTalk to perform this procedure.
You must be able to login with a user account that has been granted the
Configure Runtime Area Model Deployment
permission in the product policy configuration stored in the FactoryTalk Directory>System\Policies\Product Policies\Batch\Feature Security location.
Members of the Administrator group have this permission by default.
Then, the operator can deploy changes to the runtime area model without having to stop the
FactoryTalk Batch
Server. If the set of differences is permitted by the
FactoryTalk Batch
Server, the updated area model is successfully deployed.
TIP: An area model can also be verified and deployed from the
FactoryTalk Batch Equipment Editor
. For more information, see the
FactoryTalk Batch Equipment Editor
User Guide
.
To verify an updated area model using the FactoryTalk Batch Service Manager:
  1. Open the
    FactoryTalk Batch
    Service Manager.
  2. Select
    Verify/Deploy Area Model
    .
  3. If prompted, log on to
    FactoryTalk
    .
  4. Select an area model from the
    Updated Area Model
    list.
  5. Select
    Verify Area Model
    to compare the original area model with the updated area model.
  6. If the verification is not successful, a message displays. Select
    View Log
    to view the reason for the differences that are not permitted.
  7. Select
    Close
    .
To deploy an updated area model using the FactoryTalk Batch Service Manager:
  1. Open the
    FactoryTalk Batch
    Service Manager.
  2. Select
    Verify/Deploy Area Model
    .
  3. If prompted, log on to
    FactoryTalk
    .
  4. Select an area model from the
    Updated Area Model
    list.
  5. Select
    Deploy Area Model
    .
    The
    Status
    area displays whether the deployment is allowed. If it is not successful, a message displays. Select
    View Log
    to view the details. If the operator attempting to deploy an updated area model does not have the required
    FactoryTalk
    permissions, this button is disabled.
  6. Select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal