Download a container selection priority for the current binding
Configure the PXRQ instruction in
Logix Designer
to download the container selection priority for the material, container, feed type, and unit currently in use by this phase.External Request | Data Value Array Element | Value |
|---|---|---|
Download Container Binding Priority | DINT[0] | Phase parameter tag number. |
DINT[1] | ||
DINT[2] |
The value is stored into a specified tag.
Provide Feedback