Download data from container currently in use
Configure the PXRQ instruction to download material data from the container the phase currently runs against:
External Request | Data Value Array Element | Value |
|---|---|---|
Download Material Manager Data Container in Use | DINT[0] | 1 |
DINT[1] | Data to download (attribute ID). | |
DINT[2] | The phase parameter tag number the value downloads into. |
Provide Feedback