[ResourceID]ResourceDataX example
A client request to retrieve the value of a
[ResourceID]ResourceDataX
item could return:<ResourceDataX ID="42" Name="Reactor1007" Type="3" ArbMask="6" />
Provide Feedback