[ResourceID] ResourceDataX
The
[ResourceID]ResourceDataX
item is a set of items that correspond on a one-to-one basis with the ResourceIndexData entries (ID & Type attributes) exposed in the ResourcesListX
data item. The [ResourceID]ResourceDataX
data item returns the ID, name, type, and arbitration mask (ArbMask) of a single resource. Example Input of [ResourceID]ResourceDataX: | |
object.GetItem([ResourceID]ResourceDataX) | |
Output of [ResourceID]ResourceDataX: | |
<ResourceDataX> | |
<ResourceData> | |
</ResourceDataX> | |
where ResourceData is: | |
<ResourceDataX ID="Value" Type="Value" Name="Value" ArbMask="Value" /> | |
where : | |
ID (integer) – A unique equipment ID for a resource. Resource IDs can also be zero or negative. Zero is reserved for the operator object and negative IDs are used for recipe procedures. | |
Type (positive integer) =
| |
Name (string) – The name of the resource | |
ArbMask (nonNegativeInteger) – The arbitration mask is used as a bitmask, with each bit indicating whether a specific command is valid or invalid. | |
A client request to retrieve the value of a
[ResourceID]ResourceDataX
item could return:<ResourceDataX ID="42" Name="Reactor1007" Type="3" ArbMask="6" />
Provide Feedback