ParamExpClear
The
PARAMEXPCLEAR
execute allows the operator to remove an override of a specified expression that was created by a prior ParamExpOverride
execute. When the override clears, the current expression evaluation determines the value of the parameter expression.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[ParamExpClear( Item, UserID, ParamExpressionID )] | |
where: | Item | Name of the response item, as specified by the client. |
UserID | User identification entered into the event journal associated with this event. | |
ParamExpression-ID | Unique ID, as assigned by the system, of the parameter expression targeted by the override. The parameter expression ID is typically retrieved by a client application using the ProcedureIDData3 data item. | |
Action | A successful ParamExpClear execute removes an existing expression value force and cause the value of the expression to revert to the value to which the expression currently evaluates. | |
Return Format | The response item populates with this data: SUCCESS: | FAIL: <message> | |
where: | ||
Field Name | Format | Description |
<message> | ASCII - String | Error message appropriately formatted for operator display. |
The following table shows an example of the return on this execute.
Example: | An execute string consisting of: ParamExpClear(Item,Station2/View,27) Could return: SUCCESS: |
Provide Feedback