Binding

Binding is the process of mapping steps within a control recipe to actual equipment in a plant. Binding occurs as follows:
  • Unit binding
    is the process of selecting a unit that meets the criteria of a recipe’s unit requirement. The binding process allows the step and data references to be mapped to tags and phase programs at runtime. Unit binding is available for class-based recipes only.
  • Material phase binding
    is the process of either binding unbound material-enabled phase steps to a material phase and associated container or rebinding a previously bound material-enabled phase step within a control recipe.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal