FactoryTalk Batch default policy settings
When the
FactoryTalk
Services Platform is installed, FactoryTalk
Security product policies are created in the FactoryTalk Directory
for FactoryTalk Batch View
clients. The product policies for
FactoryTalk Batch
Clients are created in both the Local and Network Directories, except for the
Configuration Options
which are only created in the Local Directory.Provide Feedback