Service state
The 
Service State
area contains buttons, text and a graphic traffic light service
state representation. 
These server states and corresponding colors are shown:
STARTING | None |
RUNNING | Green |
STOPPED | Red |
PAUSED | Yellow |
NOT CONNECTED | None |
START PENDING | None |
The
Service State
area contains these buttons:Item | Definition |
|---|---|
Stop | Stops the selected service. |
Pause | Pauses the selected service. This button is not enabled for the batch server. |
Start/
Continue | Starts the selected service or continues a service that has been paused. |
TIP:
The state of the
FactoryTalk Batch
Service Manager (information from the Connection
and Server
groups) is
stored from the last time the Service Manager was run. These values are written when the
FactoryTalk Batch
Server is closed.Provide Feedback