Batch Service Manager server options

These methods are available to restart the
FactoryTalk Batch
Server after a service halt:
Cold Boot
Restarts the
FactoryTalk Batch
Server in a cold state. All journal data or recipe content is erased upon startup. If Security Authority is enabled, SAIs in a secured area model and any secured recipes must match the current Network
FactoryTalk Directory
SAI.
Warm Boot
Restarts the
FactoryTalk Batch
Server, restoring the set of batches that were on the batch list when the
FactoryTalk Batch
Server previously terminated. No validation for Security Authority is performed.
Warm All Boot
Restarts the
FactoryTalk Batch
Server only if it is able to restore all of the batches to the batch list. No validation for Security Authority is performed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal