Upload all reports (output parameters)
Configure the PXRQ instruction in
Logix Designer
to upload values for all configured reports to the report array:External Request | Data Value Array Element | Value |
|---|---|---|
Upload Output Parameters | DINT[0] | 0 |
If control strategies are enabled, only those reports assigned to the recipe’s control strategy are uploaded.
Provide Feedback