Single Specific Ingredient Addition Phase with no target_xx parameter
This is an example of Single Specific Ingredient Addition Phase with no target_xx parameter:
Formula Parameter: | Material_Oil |
Formula Parameter: | Setpoint_Oil |
Report Parameter: | Lot_Oil |
Report Parameter: | Actual_Lot_Oil |
Report Parameter: | Actual_Oil |
Report Parameter: | In_Tolerance_Oil |
Provide Feedback