Extended viewer message fields in FactoryTalk Diagnostics Viewer
Extended fields are provided in the
FactoryTalk
Diagnostics Viewer.Field | Data Type | Description | Used In |
|---|---|---|---|
Verbosity | Long | This value field is arbitrary; values from 1 through 100 are valid. Use to further define or filter messages. | Not used. |
Action | BSTR | The updating/editing action made by the user. | All audit messages. |
Area | BSTR | For Equipment objects, the area name the object belongs to. This field is used when needed. | Some Equipment audit messages. |
ContainingObject | BSTR | The object type that contains the EditedObject. This is used to help define exactly what object is being edited/updated. | Some Equipment audit messages. |
ContainingObjectID | BSTR | The sub-property or object property field of the equipment or recipe object affected by the action. | Some Equipment and Recipe audit messages. |
EditedObject | BSTR | The Equipment or Recipe object affected by the action. | All audit messages. |
EditedObjectID | BSTR | The most common way to identify the EditedObject. | All audit messages. |
EditedProperty | BSTR | The property affected by the action. | Some Recipe, Equipment and Area audit messages. |
EditedProperty1 | BSTR | ||
EditedProperty2 | BSTR | Preference priority | |
EquipmentPhase | BSTR | For Equipment objects, the equipment phase name the object belongs to. This field is used when needed. | Some Equipment audit messages. |
NewValue | BSTR | The value of a property after it was changed. | Updating audit events only. |
NewValue1 | BSTR | The value of a property after it was changed:
| |
NewValue2 | BSTR | Priority number | |
OldValue | BSTR | The value of a property before it was changed. | Updating audit events only. |
OldValue1 | BSTR | The value of a property before it was changed:
| Updating audit events only. |
OldValue2 | BSTR | Priority number | Updating audit events only. |
Operation | BSTR | For Recipe objects, the operation name the object belongs to. This field is used when needed. | Some Recipe audit messages. |
Procedure | BSTR | For Recipe objects, the procedure name the object belongs to. This field is used when needed. | Some Recipe audit messages. |
ProcessCell | BSTR | For Equipment objects, the process cell name the object belongs to. This field is used when needed. | Some Equipment audit messages. |
SubAction | BSTR | An updating/editing action to a list that is a property of the EditedObject. This can be Add or Delete. | Updating audit events for properties that are lists only. |
SubObject | BSTR | The object type referenced by the EditedObject. | Updating audit events for properties that are lists only. |
SubObjectID | BSTR | The value of a property after it was changed. | Updating audit events for properties that are lists only. |
Unit | BSTR | For Equipment objects, the unit name the object belongs to. This field is used when needed. | Some Equipment audit messages. |
UnitProcedure | BSTR | For Recipe objects, the unit procedure name the object belongs to. This field is used when needed. | Some Recipe audit messages. |
Working Set | BSTR | For Recipe objects, the computer name and database where the recipes are stored. | Some Recipe audit messages. |
Provide Feedback