Synchronize the area model with the project file
Use these instructions to synchronize the area model with the project file.
Prerequisite
:- InstallLogix DesignerandFactoryTalk Linxon the same computer asFactoryTalk Batch Equipment Editor.
- Create phases inFactoryTalk Batch Equipment Editorand assign aLogix5000CIP data server.
- Create a project file inLogix Designer.
- Specify this project file in theAdd or Edit Data Serverdialog box for the appropriate data server.
To synchronize the area model with the project file
:- Save the area model and select a data server to synchronize.
- Select the phases to create in theLogix Designerproject.
- Synchronize, review the results, and save the project.
All synchronization steps are completed in
FactoryTalk Batch Equipment Editor
.Provide Feedback