ResourcesListX example

A client request to retrieve the value of the
ResourcesListX
data item could return:
<ResourcesListX>
<Res ID="-82" Type="5" />
<Res ID="2" Type="1" />
<Res ID="3" Type="2" />
<Res ID="7" Type="3" />
<Res ID="20" Type="4" />
<Res ID="-83" Type="5" />
</ResourcesListX>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal