Download report limits
During batch execution, phase logic can send this request to the
FactoryTalk Batch
Server to download report limits information for all reports or for a single report.
TIP:
A report in the
FactoryTalk Batch
software is an output parameter in the Logix Designer
application.Take corrective action if a report value is outside the configured limits.
The limit configuration consists of the report’s verification method and each configured range of limits. The verification methods are written as values to the phase’s phase tags. The values for the verification methods are:
Verification Method | Value |
|---|---|
No_Limits | 0 |
High / Low | 1 |
High-High / Low-Low | 2 |
High-High-High / Low-Low-Low | 3 |
Provide Feedback