FactoryTalk Batch system configuration
The
FactoryTalk
components installation program configures the local computer with the necessary COM
Security settings to allow remote communication between the FactoryTalk
Server and client applications.The configuration of the local computer during installation depends on whether you are
installing a server or client application, a application and whether the Windows Firewall is enabled or disabled.
FactoryTalk
or e
ProcedureProvide Feedback