Arguments from the FactoryTalk Batch Server
The
FactoryTalk Batch
Server passes these arguments to the FactoryTalk Event Archiver
:<path to custom executable file> <.ini file name> <path to archque.txt> <time delay in minutes>
Example
C:\Program Files\Rockwell Software\Batch\PROJECTS\CUSTOM\MYARCHVR.EXE MYARCHVR.INI C:\Program Files\Rockwell Software\Batch\PROJECTS\JOURNALS\ARCHQUE.TXT 30
Provide Feedback