Add a member variable derived from the Phase Control Class
Use MFC to add a member variable derived from the
Phase Control Class
.
TIP:
The category is
Control
, and the variable type is the Phase Control Class
. Use the appropriate resource ID as assigned to the instance of the control in the dialog.To add a member variable derived from the Phase Control Class
:- Using the Class Wizard, add a member variable to the project’s dialog class.
- Repeat for each phase (each instance of the control).
Provide Feedback