Work with electronic batch records
An electronic batch record (
.evt
) file is a record (history) of a batch. Use this record for regulatory and reporting purposes. The ISA S88.01 standard defines batch history as a collection of data describing or related to a batch.For every batch execution, the
FactoryTalk Batch
Server creates and updates an electronic batch record (.evt
)
file during
the execution of the batch procedure. Each electronic batch record entry contains fields
entries based on event types. All data is in ASCII format, which may represent time,
integer, real number, string, or enumerations.As events occur during batch execution, the
FactoryTalk Batch
Server appends data to the batch record. Access the batch record from FactoryTalk Batch
View. The batch data is in a simple ASCII format file. View batch data with a text
editor, word processor, or spreadsheet
program.See the
ISA S88.01 Standard
for more information on modes, states, and commands.See the for more information on electronic batch records.
FactoryTalk Batch
System Files Reference GuideProvide Feedback