Upload material data into material in container currently in use
This request fails (without notice) if the data is read-only.
Configure the PXRQ instruction in
Logix Designer
to upload material data about the current material inside the container the phase currently runs against.External Request | Data Value Array Element | Value |
|---|---|---|
Upload Material Manager Data Container in Use | DINT[0] | 2 |
DINT[1] | Data to upload into. | |
DINT[2] | Report tag address of the value stored in the material database. |
Provide Feedback