CallTimeout property
The
CallTimeout
property returns or sets a value indicating the number of milliseconds the object waits for the server to return requested data before assuming that communication with the server has been lost. The CallTimeout
property applies to the BatchRemote
object.Syntax | object.CallTimeout [= value] | |
|---|---|---|
The CallTimeout property syntax has these parts: | ||
Part | Description | |
object | Object expression that evaluates to a previously defined BatchRemote.RemoteSupport object. | |
value | Numeric expression indicating the number of milliseconds the object waits for the server to return requested data before assuming that communication with the server has been lost. The default is 1000 . | |
Remarks | The data for the item returns synchronously with this method. The FactoryTalk Batch Server waits, at most, a time period equal to the TimeoutPeriod property. If the server does not recognize an item string, then strReturn contains FAILED. If the timeout period expires before the data is collected internally to the FactoryTalk Batch Server, then strReturn contains TIMEOUT. | |
This code example is
Visual Basic
6 syntax.Example: | Dimension a remote FactoryTalk Batch Server object:Dim svr As New BatchRemote.RemoteSupport Set the CallTimeout period: svr.CallTimeout = 5000 |
Provide Feedback