- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Momentary button
Button whose value is set for a minimum time (if set) or as long as it is held down, but not longer than a maximum time (if set)
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Active | Active | True if the button is held down or after a minimum hold time (if set); false if the button is released or after a maximum hold time (if set) | |
Minimum hold time | MinHoldTime | Minimum duration of active state | |
Maximum hold time | MaxHoldTime | Maximum duration of active state | |
Text | Text | (Inherited from Button) | |
Appearance | Appearance | (Inherited from Button) | |
Image path | ImagePath | (Inherited from Button) | |
Image position | ImagePosition | (Inherited from Button) | |
Text position | TextPosition | (Inherited from Button) | |
Image width | ImageWidth | (Inherited from Button) | |
Image height | ImageHeight | (Inherited from Button) | |
Word wrap | WordWrap | (Inherited from Button) | |
Text trimming | Elide | (Inherited from Button) | |
Font family | FontFamily | (Inherited from Button) | |
Font weight | FontWeight | (Inherited from Button) | |
Font italic | FontItalic | (Inherited from Button) | |
Font size | FontSize | (Inherited from Button) | |
Text color | TextColor | (Inherited from Button) | |
Background color | BackgroundColor | (Inherited from Button) | |
Style | Style | (Inherited from Button) | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Provide Feedback