- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
CODESYS Station
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Gateway IP | GatewayIP | IP address of a valid CODESYS Gateway available in the network; usually, the IP address of the controller | |
Port | Port | TCP/IP port used to connect with the controller. You can obtain the value from the CODESYS PLC Programming Environment: From the On line menu, select Communication Parameter | |
Device Name / Address | PLCAddress | The CODESYS Controller Device Name or its IP address. The IP address can refer to the same machine that runs the driver using the local IP address or localhost | |
Timeout | Timeout | Maximum wait time in milliseconds to receive a response from the controller | |
Operation code | OperationCode | (Inherited from Communication station) | |
Tags | Tags | (Inherited from Communication station) | |
Types | Types | (Inherited from Communication station) |
Provide Feedback