Data controls
    Use data controls objects to visualize data in your application interface. Get data from project nodes or a database.
Object  | Description  | 
|---|---|
Select items from a drop-down list at runtime.  | |
Select items from a list box at runtime.  | |
Display data in a table.  | |
Display trends that present values from one or more variables that are logged or read in real time.  | |
Display the value of two-dimensional variables in a graph.  | |
Display data in the form of a pie chart.  | |
Display data in the form of a bar diagram.  | 
Provide Feedback